TEST mode LED energy pulsing
Above the display screen are two pairs of energy pulsing LEDs and infrared outputs. The LEDs and IR outputs are factory-configured to pulse while the meter is in TEST mode.
|
A |
WATT infrared output |
|
B |
WATT LED |
|
C |
The Kt label indicates the default pulsing rate |
|
D |
VAR infrared output |
|
E |
VAR LED |
The energy pulsing LEDs provide an interface for accuracy checking instruments. The Kt label indicates the factory-configured pulsing rate. (You can change the energy pulsing frequency with Power Monitoring Expert or ION Setup.) See Configuring energy pulsing for more information on configuring the LED settings.