Data display
Built-in web server and webpages
Your meter’s onboard internal web server and built-in webpages provide quick and easy access to real-time energy, basic power quality information and meter configuration without having to use specialized software.
Localization
The meter can be customized to use different regional settings.
Localization settings determine:
- The language used for the display and webpages
- Time, date, and digit formats
- Displayed phase labels (123/ABC)
- Institute of Electrical and Electronics Engineers (IEEE) or International Electrotechnical Commission (IEC) conventions for power, power factor, and energy
Configure your meter’s localization settings using ION Setup or the display.
Display
Use the meter’s display to view real-time and historical power quality data, access monitoring tools, receive and acknowledge alarms, and perform basic device configuration.
The touch-screen color display has multiple mounting options to suit your environment and an eight-language interface with external LED indicators for power, alarms, and energy pulsing applications.