Configuring LPCT connected directly to conductors

I1–I3

  1. Open ION Setup > select the meter > Setup Assistant.
  2. Click Metering Setup > Basic tab.
  3. Set the LPCT CT primary value:
    1. Select PM1 CT Prim > Edit. The LVCS Configuration Setup dialog box opens.
    2. Enter the LPCT primary value.
    3. Click OK.
  4. Set the LPCT CT secondary value:
    1. Select PM1 CT Sec > Edit. The LVCS Configuration Setup dialog box opens.
    2. Enter the LPCT secondary value.
    3. Click OK.

The CT Prim and CT Sec values are stored to the device register.

I4, I5

Configure these settings in Metering Setup > Advanced tab.