Configuring EtherGate or Secure EtherGate using ION Setup
To configure EtherGate or Secure EtherGate communications using ION Setup:
- Start ION Setup.
- Open the Setup Assistant for your meter.
- Click Communications > Serial settings.
- Select the tab (Com1 or Com4) for the serial port you want to configure.
- Highlight the parameter, and then click Edit. Enter the meter password if prompted
- Change the settings, and then
click OK to save the changes.
Parameter Setting Protocol
EtherGate or Secure EtherGate
Baud Rate
Serial Port
Serial port settings must match the settings for all connected serial devices.
- Create an Ethernet gateway site to access the serial network of devices through your gateway meter.