Configuring your meter as a Modbus server using the webpages
To configure your meter as a Modbus server using the meter webpages:
- Connect to your meter’s webpages.
- Navigate to Setup > Serial Port.
- Expand Basic Settings or Advanced Settings, and then configure
the serial port’s Modbus parameters as required:
Parameter Setting Protocol
Modbus RTU or Modbus Master
RS485 Bias
- OFF if the meter is a Modbus server
- ON if the meter is a Modbus client
- Configure the meter’s other serial port parameters
as required.
Next, add the Modbus server devices using ION Setup.
See your device’s Modbus map, available from www.se.com for Modbus register information.