Ethernet communications connections
Your meter’s dual port Ethernet connections enable you to use straight-line or network loop (ring) topology.
If local network loop Ethernet topology is required, you must enable RSTP for your meter’s Ethernet communications to function.
Use CAT5 (or higher) Ethernet cables with unshielded RJ45 modular connectors to wire your meter’s Ethernet communications.
Ethernet loop topology
| A | Ethernet switch or hub |
| B | Ethernet connected meters |
| C | LAN / WAN |