Digital inputs
Digital input applications
Digital inputs are typically used for monitoring the status of switches or contacts, such as status contacts on circuit breakers.
They can also be used for pulse counting or input metering applications, such as WAGES (water, air, gas, electricity, steam) monitoring, or conditional energy applications, or IRIG-B time synchronization.
Pulse mode
If you set Input Mode to PULSE, a pulse is generated at the Trigger output when the State output changes from OFF-to-ON. No pulse is generated when State changes from ON-to-OFF.
KYZ mode
If you set Input Mode to KYZ, a pulse is generated at the Trigger output for each change of state transition, for example from OFF-to-ON and from ON-to-OFF transitions.
A/C mode
If you set Input Mode to A/C, the digital input port is configured to detect the presence of a low voltage AC signal. The next illustration shows how a digital input can be used to monitor the operation of a low voltage AC fan controller.
IRIG-B time synchronization
You can use a digital input to synchronize the meter time to an IRIG-B time source.
You can connect an IRIG-B time source to one of meter’s digital inputs for IRIG-B time synchronization. For IRIG-B time synchronization, you must configure both the meter’s digital input and the meter’s clock.
Note: For improved accuracy use the digital inputs on the meter base.