Sample setup webpage
You can create custom setup webpages using the sample webpage stored on your meter.
Sample webpages are stored in the documents folder on your meter’s internal SFTP site.
Your meter’s Modbus register map is available from www.se.com.
If required, your meter’s ION handles document is packaged with the meter firmware file which is available for download from www.se.com.
Custom setup webpages must be stored on your meter’s internal SFTP site in the web/setup folder. The custom webpage is viewed by selecting the Setup main menu tab on your meter’s webpage.
Configuring the HTML code other than where described is an advanced procedure and should only be performed by those with an advanced understanding of webpages and how your meter processes them.
Sample webpage setup result
Note: The following graphic is representative only. Your meter’s webpages may appear different than shown.
| A | HTML filename |
| B | Content pane title |
| C | Sub-heading |
| D | Row heading |
| E | Named register value |
| F | Second content pane title |