Monitoring the event log
Monitor event logs for suspicious activity and to help identify the cause of cybersecurity breaches that could lead to a cybersecurity incident.
Note: The default event log limit is 5,000 records. When the limit is reached, new log entries overwrite older ones. To be notified when the Event Log record limit is approaching, see Assigning a designated reader for event log notification. To extend log record retention, offload information to syslog or a protected storage or retention location, see Configuring Syslog network settings using ION Setup.
For more information on meter access logging events, see Editing meter access event logging.
Prerequisites:
- Meter connection using ION Setup.
- Login credentials.
To monitor the event log:
- In ION Setup, select the meter, and then open Setup Assistant.
- Click Reports > Event Log > Display.
- Select the range of records you want to view, the type, and then click OK.
- Click Save As to save the log to your local machine or print the event log.
- Click Close.