Overwriting communication module registers

  1. Open ION Setup.
  2. Ctrl + click on the meter to select it. This switches ION Setup to Advanced.
  3. Double-click Comm Modules folder > Ethernet > Setup Registers.
  4. Type text or characters to replace values for network infrastructure setup registers by selecting them and clicking Edit. Some registers include:
    • Stored IPv4 Address.
    • Stored IPv4 Subnet Mask.
    • Stored IPv4 Gateway.

      Note: IP values can be replaced with text.

    • Primary DNS.
    • Secondary DNS.
    • All servers.
    • All port numbers.
    • Ethernet Device Name.
    • Stored IPv6 Global Gateway.
    • Domain Name.
  5. Click Send.