Overwriting factory module registers
- Open ION Setup.
- Ctrl + click on the meter to select it. This switches ION
Setup to Advanced mode.
- Double-click Factory Modules folder
> select meter type.
- Select the Setup Registers tab.
- Type text or characters to replace values for these setup
registers by selecting them and click Edit:
- FAC1 Device Namespace.
- FAC1 Device Name.
- FAC1 Owner.
- FAC1 Tag1.
- FAC1 Tag2.
- Click Send.
Last updated: Friday April 11, 2025
© 2025 Schneider Electric. All Rights Reserved. Safety precautions | Disclaimer | ION9000 series help | Feedback