Setting up Advanced security
Meter security has strong user login, user access management, and password complexity.
Note: We recommend that you use Advanced security mode.
For detailed information on the Advanced security mode capabilities, see Advanced security mode.
Prerequisites:
- Meter connection using ION Setup.
- Login credentials.
- Security configuration access privileges.
To set up Advanced security:
- Open ION Setup > select the meter > Setup Assistant.
- Security > Security Mode > Edit. The Open Security Configuration file dialog box opens.
- Select the advanced.scf security configuration file.
- Click Open. If prompted, click Yes to use Advanced security.
- Next, either:
- Continue configuring the meter security settings.
- Click Finish to push your security configuration changes to the meter.