Alarm indicators
Your meter’s display has an alarm indicator to show you what alarm levels have been detected (active or historic) and whether they have been acknowledged.
For active high priority alarms, the display will also flash until the alarm is acknowledged. There is also an alarm LED to indicate the meter’s alarm condition.
| Alarm | Alarm icon | Alarm icon flash | Alarm LED | Display |
|---|---|---|---|---|
| Active high | Red solid bell | Flash if not acknowledged |
|
Flash if not acknowledged |
| Active medium | Yellow solid bell | Flash if not acknowledged |
|
No flash |
| Active low | Blue solid bell | Flash if not acknowledged |
|
No flash |
| Historic high | Red outline bell | Flash if not acknowledged |
|
No flash |
| Historic medium | Yellow outline bell | Flash if not acknowledged |
|
No flash |
| Historic low | Gray solid bell | No flash | Off | No flash |
| No active or unacknowledged alarms | Gray solid bell | No flash | Off | No flash |
If there are multiple active alarms, the alarm condition associated with the highest priority is displayed. If there are multiple unacknowledged historic alarms, the meter displays the alarm condition associated with the highest priority unacknowledged historic alarm.
Note: To stop an alarm from being displayed without impacting other metering features, set the alarm priority to Info Only.