Configuring sag/swell alarms using ION Setup
To configure sag/swell alarm settings using ION Setup:
- Start ION Setup.
- Open the Setup Assistant for your meter.
- Click Alarming > Sag/Swell.
- Select the parameter you want to configure and click Edit.
The setup dialog box for that parameter appears.
- Configure the parameters as required.
The values you need to set vary depending on the type of sag/swell alarm you are configuring.
| Parameter | Value/Range | Description |
|---|---|---|
| Enable/Disable | Enabled or Disabled |
Specifies if sag/swell recording and alarming is enabled. |
| Nominal | 1–999,999 |
The primary RMS voltage for the power system. Use the line-to-line voltage for a Delta configured device and line-to-neutral voltage for a Wye configured device. For more information on configuring Volts Mode, see Configuring metering parameters. |
| Swell Limit | Percentage of nominal | Specifies the swell limit expressed as a percentage of the nominal voltage. |
| Sag Limit | Percentage of nominal | Specifies the sag limit expressed as a percentage of the nominal voltage. |
| Hysteresis | Percentage – see description |
Specifies the difference in magnitude between the sag or swell limit and the threshold for the power quality event to be considered over. For example, if the meter has the sag limit set to 90% of nominal and the hysteresis is set to 2%, this means that in a sag event, the voltage needs to return to 92% of nominal for the sag event to be considered over |
| Alarm priority | See description |
Select the alarm priority you want to associate with Sag/Swell alarms. To stop an alarm from being displayed without affecting other meter features, set the alarm priority to Info Only. |
| Parameter | Value/Range | Description |
|---|---|---|
| Enable/Disable | Enabled or Disabled |
Specifies if sag/swell recording and alarming is enabled. |
| Nominal | 1–999,999 | Specifies the nominal current value used for current sag or current swell detection. |
| Pickup | Percentage of nominal | Specifies the percentage the current must deviate from the nominal current to be classified as a sag or a swell. |
| Dropout | Percentage of nominal | Specifies the percentage of nominal to which the current must recover to signal the end of the sag or the swell. |
| Hysteresis | N/A |
Displays the difference in magnitude between the sag or swell Pickup and Dropout values. To change the hysteresis, change the Pickup or Dropout values. |
| Alarm priority | See description |
Select the alarm priority you want to associate with Sag/Swell alarms. To stop an alarm from being displayed without affecting other meter features, set the alarm priority to Info Only. |