Disabling and enabling alarms using the display
Disable alarms using the display when you are performing maintenance tasks on your system and want to prevent nuisance alarms.
Note: To stop an alarm from being displayed without impacting other metering features, set the alarm priority to Info Only.
To disable alarms using the display:
- Press the Home button on the display.
- Press Setup Menu > Alarm Setup.
- Press Select.
- Press Edit. Enter your meter’s password, if prompted.
- Press the up or down icons to navigate alarms. A gray bar appears behind the active selection.
- To select the item(s) press Select for Enable/Disable.
- Press Select to accept the change.
- Press Select to confirm.
- Complete the system maintenance tasks.
- Enable the alarms you disabled.