Confirming subsynchronous oscillation configuration

Use ION Setup to confirm that your meter is calculating SSO results.

To confirm your subsynchronous oscillation configuration:

  1. Open ION Setup.
  2. Open advanced mode for your meter.

    If prompted, enter the device credentials.

    Tip: To open advanced mode, Ctrl+Select your meter in the Network Viewer.

  3. Select Subsynchronous Oscillation Modules.
  4. Select SSO 1 or SSO 2.
  5. Shift+Select Output Registers.

  6. Confirm that:

    1. New Update Available is non-zero, indicating that the module is operating and calculating SSO results.

    2. The number of Frequency Group N Magnitude registers matches the number of groups you defined in the Frequency Groups setup register.