Power quality standards compliance
Meter compliance
Your meter is compliant with the following power quality standards.
IEC 62586-1 and IEC 62586-2
Your meter is compliant with IEC 62586-1 and IEC 62586-2. The meter classification is PQI-A-FI1, defined as follows:
| Product Code | Description |
|---|---|
| PQI | Power quality instrument |
| A | Functions class A according to IEC 61000-4-30 |
| F | Fixed installed equipment |
| I | Indoor application |
| 1 | Indoor environment with uncontrolled temperature variations |
Note: Your meter has Power station electromagnetic immunity compliance in accordance with IEC 61000-6-5.
IEC 61000-4-30
IEC 61000-4-30 power quality standard compliance is provided by ION modules including: Power Quality Aggregator, Harmonics Measurement, Disturbance Analyzer, Symmetrical Components, Mains Signaling Evaluation, and Sag/Swell.
For more information, see the IEC 61000-4-30 compliance and ION meters technical note, available on www.se.com.
Power quality standards compliance reporting
Your meter can measure and record compliance data for the following power quality standards.
EN 50160
The EN 50160 framework includes ION modules such as Flicker, Mains Signaling Evaluation, Harmonics Evaluation, and Voltage Harmonics.
notice
data Loss
Use an Uninterruptible Power Supply (UPS) to help maintain EN 50160 framework operation during a power outage.
Failure to follow these instructions can result in data loss.
For more information about EN 50160, see the
IEEE 519
The IEEE 519 framework includes ION modules, such as: Harmonics Evaluation, Harmonics Measurement, and Counter.