Voltage crest factor
Crest factor is the ratio of peak to RMS voltage values.
For a pure sinusoidal waveform, crest factor is equal to 1.414. The meter uses the following equation to calculate crest factor:
![]() | C = Crest factor Vpeak = Voltage peak VRMS = Voltage RMS |