Verify the correct meter framework

The HSTC option is displayed as the HSTC feature set.

View the meter’s feature set using ION Setup, meter webpages, or the display.

Viewing feature set using ION Setup

  1. Open ION Setup and select the Setup Assistant for your meter.
  2. Click Template > Save to PC > FAC1 Feature Set.

Viewing feature set using the meter webpages

  1. Open a web browser and enter the IP address for your meter. Enter your login credentials when prompted.
  2. Click Diagnostics > Statistics > Meter - Basic > Feature Set.

Viewing feature set using the display

Select Alt Display Mode > Nameplate > Feature Set.

See Display modes for information about display modes.