Legacy security support
Legacy security support is an interim solution for users that use Standard security mode and is the default setting for new meters. It provides backwards compatibility with older software communicating with the meter using ION protocol.
If Standard security was used before upgrading meter firmware to v3.0.0, Legacy security support is enabled.
If Advanced security was used before upgrading meter firmware to v3.0.0, Advanced security is enabled.
Recommendation: Use Advanced security mode.
| Legacy security support username | Legacy security support password | Legacy security support password range | Legacy security support password limit |
|---|---|---|---|
| User1 |
|
0–99999999 | 8 characters |
Switch ION Setup into Advanced mode to setup multiple user accounts for meters using Legacy security support: Open ION Setup > Ctrl + click on the meter to select it.