Status
After all required meter firmware updates are complete, ION Setup continues to perform the remaining updates.
- If you selected to upgrade the template, ION Setup will paste the template into the meter.
- If you selected to upgrade PM89RD96 remote display firmware, ION Setup will perform the display upgrade through the connected DIN rail-mounted meter.