Anti-tamper sealing
The meter has several anti-tamper sealing points which can be sealed by a wire seal or lock.
In certain countries, the meter is no longer revenue certified if the anti-tamper seals are broken.
See your meter’s installation guide for sealing point locations.
notice
LOSS of COMPLIANCE
Re-certify your meter with the appropriate revenue metering authorities if you remove the anti-tamper seals.
Failure to follow these instructions may render your device non-compliant for billing purposes.
Revenue lock switch seal