Setting up Advanced security troubleshooting
Some users could experience software access issues after enabling Advanced Security mode. Resolve software access issues using these troubleshooting steps:
| Meter state | Example behavior | Solution – follow tasks in the order listed | 
|---|---|---|
| New meter | Login credentials are unknown. | 
 | 
| Meter recently upgraded to firmware v3.0.0 | Using EcoStruxure™ Power Monitoring Expert software and after password is entered, access is not granted. | 
 | 
| Using Vista software and after password is entered, access is not granted. | Go to www.se.com and search for support to get assistance with troubleshooting. | |
| Using EcoStruxure™ Power Operation software. | Go to www.se.com and search for support to get assistance with troubleshooting. | |
| Incorrect credentials are entered multiple times and a lockout occurs. | Wait until lockout duration is over and account is not locked out. If a user account is locked out, that user can still access the device by entering the correct credentials over a different protocol and communications method. | |
| Login credentials are unknown. | 
 |