Meter configuration

ION Setup device configuration tool

ION Setup is a free configuration tool for your meter that lets you remotely configure your meter’s features over Ethernet or serial communications.

  • Use the setup screens to guide you through the process of configuring your meter.
  • Use the real-time data screens to verify your meter’s configuration.
  • Use the data screens to view your meter’s recorded data.
  • Use the charting function to view your meter’s recorded waveforms.
  • Use ION Setup in Advanced mode to work directly with modules.

Download ION Setup from www.se.com.

Switching ION Setup to Advanced mode

  1. Open ION Setup.
  2. Ctrl + click on the meter to select it. This switches ION Setup to Advanced mode.