Configuring metering parameters
Use ION Setup to configure the meter’s metering functionality.
- Start ION Setup and open the Setup Assistant for your meter.
- Configure the parameters in Metering Setup > Basic.
- Configure the parameters in Metering
Setup > Advanced, if
appropriate.
Advanced tab Parameter Values Description PhaseOrder ABC, ACB Power system’s rotation order of voltage phases I4 Prim 1–999,999 I4 current transformer's primary winding current rating I4 Sec 1–999,999 I4 current transformer's secondary winding current rating Scale Rev Param ON, OFF Specifies whether revenue readings are presented as primary or secondary side values (ON = primary side, OFF = secondary side)
1 Demo mode is for demonstration only, and does not use the meter input terminals to display values.