Factory default settings
Use these default values the first time you connect to your meter.
Parameter | Default value |
---|---|
Username to log onto meter webpages | USER1 |
Password to log onto meter webpages or access display | 0 |
IP address1 | 169.254.0.10 |
Subnet mask | 255.255.0.0 |
Gateway | 0.0.0.0 |
RS-485 |
COM1 Unit ID: 100 |
Language | English |
1 The IPv6 link local address can also be used. See Self-discovery over Ethernet for details.