Changing web protocol settings using ION Setup
Web protocol settings | Description |
---|---|
HTTPS With HTTP Redirect | Redirects all HTTP requests to use HTTPS. |
HTTPS | Allows only secure access and encrypted communications between the client computer and the meter’s internal web server hosting webpages. |
Disabled | Turns off the meter’s web functionality and blocks all access to the meter’s web server. |
To change web protocol settings using ION Setup:
- Open ION Setup and select the Setup Assistant for your meter.
- Click Communications > Advanced Ethernet > Protocols tab.
- Select the Web protocol and click Edit.
- Select a web protocol setting.
- Change the default Assigned Port Numbers for HTTPS With HTTP Redirect and HTTPS. This requires appending the changed port number for HTTPS access to the meter’s webpages, for example: <meter IP address>:<changed https port number>.