Communications
Communications is the transfer of data to and from the meter and is controlled by a combination of hardware and software components in the meter.
Your meter’s default protocol settings meet the needs of most systems with only basic configuration. You can customize these settings to meet your specific needs. These are advanced procedures that require an understanding of your meter’s architecture, supported protocols, and the communications network and power system that your meter is connected to.
Topics in this section: