Configuring SNMP using ION Setup
You can enable SNMP and configure SNMP trapping using ION Setup.
Download the ION MIB file from www.se.com.
To configure SNMP using ION Setup:
- Start ION Setup.
- Open the Setup Assistant for your meter.
- Click Communications > Advanced Ethernet > SNMP.
- Configure your meter’s SNMP parameters by selecting
the parameter and clicking Edit. Click OK in the editing screen to set the parameter value.
Parameter Description Enable SNMP Enables or disables SNMP on your meter. Enable Traps Enables or disables SNMP trapping on your meter. Trap Rcvr1 Addr to Trap Rcvr4 Addr Enter up to four trap receiver IP addresses where trap messages will be sent. Read only community Enter the community string used for SNMP get (read-only) requests. Read write community Enter the community string used for SNMP set (read/write) requests. Note: You can use the read/write community string for SNMP get (read-only) requests.
System contact Enter the name of your SNMP system administrator. System name Enter a descriptive name for your meter. System location Enter your meter’s location. - Review the rest of the SNMP information and modify if necessary.