Confirming your MQTT connection

Use ION Setup to confirm that you have an active connection with the MQTT broker.

To confirm your MQTT connection:

  1. Open ION Setup.
  2. Open advanced mode for your meter.

    If prompted, enter the device credentials.

    Tip: To open advanced mode, Ctrl+Select your meter in the Network Viewer.

  3. Select MQTT Export Modules.
  4. Select MQTT Export 1.
  5. Shift+Select Output Registers.

    Status indicates the connection status:

    • True: The meter is connected to the MQTT broker.

    • False: The meter is not connected to the MQTT broker.