SFTP folders and file permissions
SFTP folder structure:
| Folder | Description |
|---|---|
| COMTRADE_1 to COMTRADE_3 | View COMTRADE files from these folders. Users have read permission of files. |
| documents | Add any file type to this folder. Users have full control of files. |
| IEC61850 | Add an IEC 61850 configuration (CID) file to this folder to activate IEC 61850 functionality. Users have full control of files in the root and read permission of files in the log folder. |
| optionModuleUpg and rmdUpg | Upload firmware upgrade files for your meter’s display or option modules to these folders. Users have full control of files. |
| web | Add custom webpages to the meter by transferring them into web subfolders. This folder is where default meter webpages are stored. Users have full control of files. |