Your meter as a Modbus client with Ethernet Modbus server devices

Your meter can function as a Modbus client with Ethernet Modbus server devices.

A Ethernet
B Your meter
C Modbus servers

To use the Modbus client-server architecture, add the Modbus server devices using ION Setup.