Configuring option module digital outputs using ION Setup

To configure the option module digital outputs using ION Setup:

  1. Start ION Setup.
  2. Open the Setup Assistant for your meter.
  3. Select Expansion Modules > Option Modules.
  4. Select the module tab that corresponds to the option module with the digital output you want to configure.

    Tip: The tabs correspond to the slot in which the option module is installed. For more information, see Option modules.

  5. Select the digital output channel and then select Edit.

    The setup screen for that digital output is displayed.

  6. Configure the digital output by selecting a parameter and then selecting Edit.

    After configuring a parameter, select OK to save the setting to the meter.

    Parameter Value/Range Description
    Source Digital/Boolean

    Link this input to the value that drives the state of the digital output.

    If Source is not linked, the digital output state is driven by the Force ON, Force OFF values.

    Force ON Pulse Link this input to a pulse that forces the digital output on for the PulseWidth duration, regardless of the Source input.
    Force OFF* Pulse Link this input to a pulse that forces the digital output off.
    Normal* Pulse Pulsing this input will switch the driver of the digital output from Force ON to Source.
    EventLog Mode Log Off/Log On Specifies if events generate log entries.
    Polarity Inverting/non-inverting Specifies if the signal to the digital port is inverted or not inverted.
    PulseWidth 0–2,000,000

    Specifies the duration of the pulse, in seconds.

    Setting this parameter to 0 sets the digital output continuously on.

    Port - The physical digital output port connection. Only available ports are shown.

    * These parameters are only valid when pulse width is set to 0.

  7. Select Send.