Alarm icon
The alarm icon indicates the highest level and state of alarms detected by your meter.
For example, if the meter detects a low priority and a high priority active alarm, the alarm icon indicates a high priority active alarm.
Note: Alarms can only be viewed and acknowledged through the display.
Icon | Description |
---|---|
![]() |
Active alarm indicator:
The alarm indicator flashes until you acknowledge the alarm. The alarm indicator changes to the historic alarm indicator of the appropriate level when the alarm state is no longer detected by the meter. Note: The display backlight flashes for unacknowledged high priority active alarms. |
![]() |
Unacknowledged historic alarm indicator:
Note: Low priority historical alarms are not indicated. The active alarm indicator changes to the historic alarm indicator of the appropriate level when the alarm state is no longer detected by the meter. |
![]() |
Gray: no active or unacknowledged high or medium priority historic alarms |