Data display screens
Your meter’s default display screens show measured and calculated information about the power system being monitored.
Menu | Submenu | Content |
---|---|---|
Summary | Summary | Power system summary. |
Alarms | Active alarms | Active alarms can be viewed and acknowledged. |
Historical alarms | Historical alarms can be viewed and acknowledged. | |
Basic readings | Voltage |
|
Current | ||
Frequency | ||
Power | Power summary |
Per-phase and total kW, kVAR and kVA values, along with minimum and maximum values. |
Demand | Delivered and received demand values including peak demand. | |
Power factor | Per-phase and total power factor along with minimum and maximum values. | |
Energy | Energy | Energy delivered-received, delivered and received. |
Events | Events | Meter event log entries listing and details. |
Power quality | EN50160 |
EN50160 values. Available on: Advanced and Standard |
Harmonics | Voltage and current harmonics, with individual and total harmonic values. | |
Phasors |
Phasor diagram with magnitude and angle values. |
|
Inputs/outputs | Digital inputs | Digital and analog I/O values and counts. |
Digital outputs | ||
Analog inputs | ||
Analog outputs | ||
Nameplate | Nameplate |
|
Custom screens | - | Custom screens. |
Setup Menu | - | Access to the setup menu screens. |