Overwriting communication module registers
- Open ION Setup.
- Ctrl + click on the meter to select it. This switches ION Setup to Advanced.
- Double-click Comm Modules folder > Ethernet > Setup Registers.
- Type text or characters to replace values for network infrastructure
setup registers by selecting them and clicking Edit. Some registers include:
- Stored IPv4 Address.
- Stored IPv4 Subnet Mask.
- Stored IPv4 Gateway.
Note: IP values can be replaced with text.
- Primary DNS.
- Secondary DNS.
- All servers.
- All port numbers.
- Ethernet Device Name.
- Stored IPv6 Global Gateway.
- Domain Name.
- Click Send.