Overwriting the meter template file
- Go to www.se.com and search for the meter template for your device.
- Download the ZIP file and extract files.
- Open ION Setup.
- Click the meter to select it > Setup Assistant.
- Click Template > Send to Meter tab.
- Click Send.
- Navigate to the extracted files and select the DCF file.
Note: FWN file type is also an option.
- Click Open.
- Click Proceed. The Template Paste Options dialog box opens.
- Clear all check boxes and click OK.
- Click Yes. The overwriting process could take a few minutes.
- Click OK.
- Click Exit and then OK.