Pushing updated security settings to the meter
After you have completed configuring the meter security settings, push the updated settings to the meter.
To push the updated security settings to the meter:
- In the ION Setup Security wizard, click Next until you reach the Security wizard pane that has a Finish button.
- Click Finish. A Confirmation message box opens.
- Click Yes to confirm your changes.
ION Setup pushes your security configuration changes to the meter.
Next, store the Security Configuration File.