Restoring default security configuration
notice
data Loss
Record your device's user and password information in a secure location.
Failure to follow these instructions can result in loss of data.
- Open ION Setup > select the meter > Setup Assistant.
- Click Security > Security Mode > Edit. The Open Security Configuration file dialog box opens.
- Select the standard.scf and click Open. If prompted, click No to use Legacy security support.
- Click Next to navigate to the Define individual users/passwords screen.
- Click Finish. The Confirmation message box opens.