Alarm types
Your meter has four types of alarms:
| Alarm type | Description |
|---|---|
| Setpoint (standard) |
Setpoint alarms compare the actual value of a parameter to a specified limit or range of values. These include measured voltage and current values and calculated power quality values. Some setpoint alarms use high-speed measurements for up to 1 millisecond resolution. |
| Digital | Digital alarms are triggered on a digital input’s on/off state. |
| Disturbance (sag/swell) | Disturbance alarms are triggered on a measured sag or swell. |
| Unary | Unary alarms are not configurable and generate an alarm based on the meter’s state, for example, the meter powering up. |
Alarms have two states:
| Alarm state | Description |
|---|---|
| Active |
The meter detects the alarm condition is met. |
| Historical | The alarm condition previously existed but the condition has since returned to a non-alarm state. |
For more information on Setpoint, Relative Setpoint, Digital Input, Disturbance Analyzer, and Sag/Swell modules, see ION Reference Help.