Alarm types

Your meter has four types of alarms:

Alarm type Description
Setpoint (standard)

Setpoint alarms compare the actual value of a parameter to a specified limit or range of values. These include measured voltage and current values and calculated power quality values.

Some setpoint alarms use high-speed measurements for up to 1 millisecond resolution.

Digital Digital alarms are triggered on a digital input’s on/off state.
Disturbance (sag/swell) Disturbance alarms are triggered on a measured sag or swell.
Unary Unary alarms are not configurable and generate an alarm based on the meter’s state, for example, the meter powering up.

Alarms have two states:

Alarm state Description
Active

The meter detects the alarm condition is met.

Historical The alarm condition previously existed but the condition has since returned to a non-alarm state.

For more information on Setpoint, Relative Setpoint, Digital Input, Disturbance Analyzer, and Sag/Swell modules, see ION Reference Help.