Disabling and enabling alarms using the display

Disable alarms using the display when you are performing maintenance tasks on your system and want to prevent nuisance alarms.

Note: To stop an alarm from being displayed without impacting other metering features, set the alarm priority to Info Only.

To disable alarms using the display:

  1. Press the Home button on the display.
  2. Press Setup Menu > Alarm Setup.
  3. Press Select.
  4. Press Edit. Enter your meter’s password, if prompted.
  5. Press the up or down buttons to navigate alarms. A gray bar appears behind the active selection.
  6. To select the item(s) press the up and down buttons simultaneously.
  7. Press Select to accept the change.
  8. Press Select to confirm.
  9. Complete the system maintenance tasks.
  10. Enable the alarms you disabled.