COMTRADE

The meter provides waveforms in COMmon format for TRAnsient Data Exchange (COMTRADE) format. IEC 60255-24 defines the COMTRADE format. COMTRADE files simplify the retrieval, analysis, and exchange of power quality event (disturbance) data between many sources and vendors.

COMTRADE records are generated from the existing Waveform Recorder modules that are connected to the COMTRADE module.

Your meter can generate COMTRADE files and store them on the meter’s internal SFTP site.

COMTRADE can be used in conjunction with IEC 61850.

For more information, see the COMTRADE and ION technology technical note, available on www.se.com.