Current crest factor
Crest factor is the ratio of peak to RMS current values.
For a pure sinusoidal waveform, crest factor is equal to 1.414. The meter uses the following equation to calculate crest factor:
![]() | C = Crest factor Ipeak = Current peak IRMS = Current RMS |