Configuring data logging using ION Setup

Use ION Setup to configure the meter’s data recorders.

Changing the meter’s data recorder configuration clears existing data in that data recorder.

notice

data Loss

Ensure that all important data is recorded before configuring data recording.

Failure to follow these instructions can result in data loss.

 

To configure data logging using ION Setup:

  1. Start ION Setup.
  2. Open the Setup Assistant for your meter.
  3. Click Logging > Memory.
  4. In the Status tab, select the data log and click Edit.

    The Log Depth Setup window appears.

  5. Configure the settings as applicable:
    ParameterDescription
    Log IntervalHow frequently records are logged
    Log DepthMaximum number of records stored in the log
    Log MemoryInformation only. This is automatically calculated, and displays how much memory the log uses based on the Log Interval and Log Depth
    Log StorageInformation only. This is automatically calculated, and displays how much total memory is left after subtracting the Log Memory usage