Configuring Syslog network settings using ION Setup
To configure Syslog network settings using ION Setup:
- Start ION Setup.
 - Open the Setup Assistant for your meter.
 - Click Communications > Advanced Ethernet > SysLog.
 - Select Enable Syslog and click Edit.
 - Select Yes to enable the syslog server feature or select No to disable it.
 - Click OK.
 - Select Syslog Server and click Edit.
 - Enter the IPv4 address or an IPv6 address for the syslog
server. 
Note: You must enter the IP address for the syslog server, not the server’s fully-qualified domain name.
 - Click OK.
 - Verify that the Syslog server is receiving log information
from the meter.
Note: If the Enable Syslog register is enabled but the Syslog Server register does not contain an IP address, an event is generated in the event log to indicate that syslog is enabled with no server IP.