Restarting the meter using the display

You can restart your device using the display to help troubleshoot issues.

Note: The device will be unavailable during the restart.

Prerequisites:

  • User with security configuration access.

Performing a restart using the display

warning

HAZARD OF unintended operation

Do not use the meter for critical control or protection applications where human or equipment safety relies on the operation of the control circuit.
Be aware that an unexpected change of state of the digital outputs may result when the supply power to the meter is interrupted or after a meter firmware or template upgrade.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

 

To perform a restart using the display:

  1. Open Setup Menu.

    Tip: To open the Setup Menu, select , and then scroll to Setup Menu.

  2. Scroll to Meter Restart, and then select .

  3. If prompted, enter the device credentials, and then select OK.

  4. Select to confirm the Meter Restart.

Verifying the meter restarted

After performing a Meter Restart, verify that the meter restarted by finding the logged meter restart event.

To find a logged meter restart event using the display:

  1. Select .

  2. Use the navigation buttons to scroll to Events, and then select .

  3. Select the latest event, and then select .

    Tip: The first event in the list is the latest event.

  4. Confirm that the event details includes:

    • Date

    • Time

    • Source: Front Panel

    • Event: Meter restart

      Note: The date and time event details should match when you performed a the meter restart.