Protected features and settings

Your revenue meter has features and settings that cannot be changed while revenue-locked.

In order to prevent changes to revenue-related features, settings and meter data, you can apply revenue-locking after all revenue-metering setup is complete. See the ION Device Template Reference, available from www.se.com, for a complete listing of revenue-locked features and settings.