Revenue locking your meter
You can lock and unlock your meter using the revenue lock switch located on the meter base.
danger
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
- Apply appropriate Personal Protective Equipment (PPE) and follow safe electrical work practices. See NFPA 70E, CSA Z462 or other local standards.
- Turn off all power supplying this device and the equipment in which it is installed before working on or in the equipment.
- Always use a properly rated voltage sensing device to confirm that all power is off.
Failure to follow these instructions will result in death or serious injury.
- Open the revenue lock switch cover.
- Locate the revenue lock switch.
- Toggle revenue lock switch on or off.
- Close the revenue lock switch cover and make sure it is firmly in place.
- Seal the revenue lock switch cover if required.