Method 1: Installing using a firmware package – recommended
The firmware package includes the most recent template and webpages to help ensure that your device has the latest features.
Any digital and analog outputs associated with your device might change state during firmware installation or when applying a template.
warning
unintended operation
Do not use this device for critical control or protection of persons, animals, property, or equipment.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
Installing firmware or applying a template onto your device clears all previously recorded data.
notice
DATA LOSS
Ensure that all important data has been recorded before uploading firmware or a template to your device.
Failure to follow these instructions can result in data loss.
Prerequisites
- Open the device table of contents
- Connect to your device
- Firmware package (.zip)
- (Optional) A device template (.fwn or .dcf) if you do not want to upgrade using the default template
To install a device firmware package:
- Select Device Management > Update > Firmware.
- Go to Install Firmware.
- Drag the firmware package (.zip) into the upload area or select Browse and then choose the firmware package.
- Read the package notes and then select Proceed.
- Select the package contents that you want to install.
- Select Proceed.
- Read the Firmware Installation Alert and then select Proceed.
- Select the template settings that you want to retain from the current template.
- Select Apply to install the device firmware.
Note: If you do not select the default template for your device from the firmware package, you will be prompted to upload a template.